Last login: Wed Aug  3 18:14:34 2022 from 192.168.68.163

root@keembay:~# gst-inspect-1.0 kmbcamsrc

KMB_ERR:  kmb_media_populate_eeprom_devices:239 Read eeprom device id /sys/bus/i2c/devices//0-0050/of_node/phandle does not have phandle 

Factory Details:
  Rank                     primary (256)
  Long-name                Generic bin
  Klass                    Generic/Bin
  Description              Simple container object
  Author                   Erik Walthinsen <omega@cse.ogi.edu>,Wim Taymans <wim.taymans@gmail.com>

Plugin Details:
  Name                     kmbcamera
  Description              Source element for Keembay camera. 
                           The element can have a different number of output pads streaming data,
                           depending on the properties set. If multi-camera-ids property is not used,
                           then only a single camera will streaming on 1 to 3 pads.
                           The camera-id property can be used to select a camera. transform-hub property
                           is used to select the amount of outputs from a given camera.
  Filename                 /usr/lib/gstreamer-1.0/libkmbcamera.so
  Version                  1.0.0
  License                  LGPL
  Source module            kmbcamera
  Binary package           Keembay Camera
  Origin URL               Intel Corporation

GObject
 +----GInitiallyUnowned
       +----GstObject
             +----GstElement
                   +----GstBin
                         +----KmbCamSrc

Implemented Interfaces:
  GstChildProxy
  KmbCamera

Pad Templates:
  none

Element has no clocking capabilities.
Element has no URI handling capabilities.

Pads:
  SRC: 'ghostSrc_0'
  SRC: 'ghostSrc_1'
  SRC: 'ghostSrc_2'
  SRC: 'ghostSrc_3'
  SRC: 'ghostSrc_4'
  SRC: 'ghostSrc_5'
  SRC: 'ghostSrc_raw'
  SRC: 'auxiliary_1_ghostSrc_0'
  SRC: 'auxiliary_1_ghostSrc_1'
  SRC: 'auxiliary_1_ghostSrc_2'
  SRC: 'auxiliary_1_ghostSrc_3'
  SRC: 'auxiliary_1_ghostSrc_4'
  SRC: 'auxiliary_1_ghostSrc_5'
  SRC: 'auxiliary_1_ghostSrc_raw'
  SRC: 'auxiliary_2_ghostSrc_0'
  SRC: 'auxiliary_2_ghostSrc_1'
  SRC: 'auxiliary_2_ghostSrc_2'
  SRC: 'auxiliary_2_ghostSrc_3'
  SRC: 'auxiliary_2_ghostSrc_4'
  SRC: 'auxiliary_2_ghostSrc_5'
  SRC: 'auxiliary_2_ghostSrc_raw'
  SRC: 'auxiliary_3_ghostSrc_0'
  SRC: 'auxiliary_3_ghostSrc_1'
  SRC: 'auxiliary_3_ghostSrc_2'
  SRC: 'auxiliary_3_ghostSrc_3'
  SRC: 'auxiliary_3_ghostSrc_4'
  SRC: 'auxiliary_3_ghostSrc_5'
  SRC: 'auxiliary_3_ghostSrc_raw'

Element Properties:
  ae-antibanding      : AE antibanding property defines which antibanding mode will be used
                        flags: readable, writable
                        Enum "KmbCamAEAntibanding" Default: 0, "off"
                           (0): off              - KMB_CAMERA_AE_ANTIBANDING_MODE_OFF
                           (1): 50HZ             - KMB_CAMERA_AE_ANTIBANDING_MODE_50HZ
                           (2): 60HZ             - KMB_CAMERA_AE_ANTIBANDING_MODE_60HZ
                           (3): AUTO             - KMB_CAMERA_AE_ANTIBANDING_MODE_AUTO
  ae-convergence-speed: AE convergence speed property sets convergence speed
                        flags: readable, writable
                        Enum "KmbCamAEConvergenceSpeed" Default: 0, "normal"
                           (0): normal           - KMB_CAMERA_AE_CONVERGENCE_SPEED_NORMAL
                           (1): medium           - KMB_CAMERA_AE_CONVERGENCE_SPEED_MEDIUM
                           (2): low              - KMB_CAMERA_AE_CONVERGENCE_SPEED_LOW
  ae-exposure-compensation: Adjustment to autoexposure target image brightness
                        flags: readable, writable
                        Integer. Range: -2147483648 - 2147483647 Default: 0 
  ae-lock             : Whether autoexposure is currently locked to its latest calculated values
                        flags: readable, writable
                        Enum "KmbCamAELock" Default: 0, "off"
                           (0): off              - KMB_CAMERA_AE_LOCK_OFF
                           (1): on               - KMB_CAMERA_AE_LOCK_ON
  ae-mode             : Whether autoexposure is currently updating the sensor exposure and sensitivity fields
                        flags: readable, writable
                        Enum "KmbCamAEMode" Default: 0, "off"
                           (0): off              - KMB_CAMERA_AE_MODE_OFF
                           (1): on               - KMB_CAMERA_AE_MODE_ON
                           (2): auto-flash       - KMB_CAMERA_AE_MODE_ON_AUTO_FLASH
                           (3): always-flash     - KMB_CAMERA_AE_MODE_ON_ALWAYS_FLASH
                           (4): flash-redeye     - KMB_CAMERA_AE_MODE_ON_AUTO_FLASH_REDEYE
  ae-precapture-trigger: Whether the 3A Framework must trigger precapture metering
                        flags: readable, writable
                        Enum "KmbCamAEPrecaptureTrigger" Default: 0, "idle"
                           (0): idle             - KMB_CAMERA_AE_PRECAPTURE_TRIGGER_IDLE
                           (1): start            - KMB_CAMERA_AE_PRECAPTURE_TRIGGER_START
  ae-regions          : Comma separated values for setting AE regions following the rule:
                        {left, right, top, bottom, weight}
                        or with multiple regions:
                        {left1, right1, top1, bottom1, weight1, left2, right2, top2, bottom2, weight2, ...}
                        flags: readable, writable
                        String. Default: ""
  af-mode             : Whether autofocus is currently enabled, and what mode it is set to
                        flags: readable, writable
                        Enum "KmbCamAFMode" Default: 0, "off"
                           (0): off              - KMB_CAMERA_AF_MODE_OFF
                           (1): auto             - KMB_CAMERA_AF_MODE_AUTO
                           (2): macro            - KMB_CAMERA_AF_MODE_MACRO
                           (3): continuous-video - KMB_CAMERA_AF_MODE_CONTINUOUS_VIDEO
                           (4): continuous-picture - KMB_CAMERA_AF_MODE_CONTINUOUS_PICTURE
                           (5): edof             - KMB_CAMERA_AF_MODE_EDOF
  af-trigger          : Whether the 3A Framework must trigger autofocus
                        flags: readable, writable
                        Enum "KmbCamAFTrigger" Default: 0, "idle"
                           (0): idle             - KMB_CAMERA_AF_TRIGGER_IDLE
                           (1): start            - KMB_CAMERA_AF_TRIGGER_START
                           (2): cancel           - KMB_CAMERA_AF_TRIGGER_CANCEL
  async-handling      : The bin will handle Asynchronous state changes
                        flags: readable, writable
                        Boolean. Default: false
  auto-hdr-enable     : Enable auto HDR feature
                        flags: readable, writable
                        Boolean. Default: false
  awb-lock            : Whether auto-whitebalance is currently locked to its latest calculated values
                        flags: readable, writable
                        Enum "KmbCamAWBLock" Default: 0, "off"
                           (0): off              - KMB_CAMERA_AWB_LOCK_OFF
                           (1): on               - KMB_CAMERA_AWB_LOCK_ON
  awb-mode            : Whether auto-whitebalance is currently setting the color transform fields, and what its illumination target is
                        flags: readable, writable
                        Enum "KmbCamAWBMode" Default: 0, "off"
                           (0): off              - KMB_CAMERA_AWB_MODE_OFF
                           (1): auto             - KMB_CAMERA_AWB_MODE_AUTO
                           (2): incadescent      - KMB_CAMERA_AWB_MODE_INCANDESCENT
                           (3): fluorescent      - KMB_CAMERA_AWB_MODE_FLUORESCENT
                           (4): warm-fluorescent - KMB_CAMERA_AWB_MODE_WARM_FLUORESCENT
                           (5): daylight         - KMB_CAMERA_AWB_MODE_DAYLIGHT
                           (6): cloudy-daylight  - KMB_CAMERA_AWB_MODE_CLOUDY_DAYLIGHT
                           (7): twilight         - KMB_CAMERA_AWB_MODE_TWILIGHT
                           (8): shade            - KMB_CAMERA_AWB_MODE_SHADE
  awb-regions         : Comma separated values for setting AWB regions following the rule:
                        {left, right, top, bottom, weight}
                        or with multiple regions:
                        {left1, right1, top1, bottom1, weight1, left2, right2, top2, bottom2, weight2, ...}
                        flags: readable, writable
                        String. Default: ""
  calib-src           : Calibration source options: 0, 1. Select reading  data source where 0 is EEPROM IC, 1 is File located.at /usr/bin/ with name calib_data_{cam_id}.bin
                        flags: readable, writable
                        Unsigned Integer. Range: 0 - 4294967295 Default: 0 
  camera-id           : (0): kmb-imx412-sensorkeembay_cam_a
                        (1): kmb-ov9282-sensorkeembay_camex_
                        (2): kmb-ov9282-sensorkeembay_camex_
                        (3): kmb-ov9282-sensorkeembay_cam_ve
                        
                        flags: readable, writable
                        Unsigned Integer. Range: 0 - 3 Default: 0 
  camera-mode         : Camera mode property. Supported values are: ull, HDR-2DOL, HDR-3DOL, mono, no-isp
                        flags: readable, writable
                        String. Default: "ull"
  capture-intent      : Information to 3A routines about the purpose of this capture, to help decide optimal 3A strategy
                        flags: readable, writable
                        Enum "KmbCamCaptureIntent" Default: 0, "preview"
                           (0): preview          - KMB_CAMERA_CAPTURE_INTENT_PREVIEW
                           (1): capture          - KMB_CAMERA_CAPTURE_INTENT_STILL_CAPTURE
                           (2): video-record     - KMB_CAMERA_CAPTURE_INTENT_VIDEO_RECORD
                           (3): video-snapshot   - KMB_CAMERA_CAPTURE_INTENT_VIDEO_SNAPSHOT
                           (4): zsl              - KMB_CAMERA_CAPTURE_INTENT_ZERO_SHUTTER_LAG
  control-adapter     : Property to choose a control adapter type. Valid values are: guzzi, guzzi_live_tuning, legacy, sim
                        flags: readable, writable
                        String. Default: "guzzi"
  edge-mode           : Operation mode for edge enhancement
                        flags: readable, writable
                        Enum "KmbCamEdgeMode" Default: 0, "off"
                           (0): off              - KMB_CAMERA_EDGE_MODE_OFF
                           (1): on               - KMB_CAMERA_EDGE_MODE_ON
  edge-strength       : Control the amount of edge enhancement applied to the images
                        flags: readable, writable
                        Integer. Range: 1 - 10 Default: 0 
  effect-mode         : Whether any special color effect is in use
                        flags: readable, writable
                        Enum "KmbCamEffectMode" Default: 0, "off"
                           (0): off              - KMB_CAMERA_EFFECT_MODE_OFF
                           (1): mono             - KMB_CAMERA_EFFECT_MODE_MONO
                           (2): negative         - KMB_CAMERA_EFFECT_MODE_NEGATIVE
                           (3): solarize         - KMB_CAMERA_EFFECT_MODE_SOLARIZE
                           (4): sepia            - KMB_CAMERA_EFFECT_MODE_SEPIA
                           (5): posterize        - KMB_CAMERA_EFFECT_MODE_POSTERIZE
                           (6): whiteboard       - KMB_CAMERA_EFFECT_MODE_WHITEBOARD
                           (7): blackboard       - KMB_CAMERA_EFFECT_MODE_BLACKBOARD
                           (8): aqua             - KMB_CAMERA_EFFECT_MODE_AQUA
  enable-metadata-debug: Enable ISP cfg copy in metadata
                        flags: readable, writable
                        Boolean. Default: false
  flash-firing-power  : Power for flash firing/torch
                        flags: readable, writable
                        Integer. Range: 0 - 10 Default: 0 
  flash-firing-time   : Firing time of flash relative to start of exposure
                        flags: readable, writable
                        Integer. Range: -2147483648 - 2147483647 Default: 0 
  flash-mode          : Flash mode defines how the flash light should be used
                        flags: readable, writable
                        Enum "KmbCamFlashMode" Default: 0, "off"
                           (0): off              - KMB_CAMERA_FLASH_MODE_OFF
                           (1): signal           - KMB_CAMERA_FLASH_MODE_SINGLE
                           (2): torch            - KMB_CAMERA_FLASH_MODE_TORCH
  flash-trigger       : Flash trigger defines on which frame flash light should be activated
                        flags: readable, writable
                        Integer. Range: -2147483648 - 2147483647 Default: 0 
  frame-flip          : Enable frame flip
                        flags: readable, writable
                        Integer. Range: 0 - 1 Default: 0 
  frame-mirror        : Enable frame mirror
                        flags: readable, writable
                        Integer. Range: 0 - 1 Default: 0 
  frame-rotation      : Frame rotation property defines video rotation
                        flags: readable, writable
                        Enum "KmbCamFrameRotation" Default: 0, "0"
                           (0): 0                - KMB_CAMERA_VIDEO_ROTATION_0
                           (1): 90               - KMB_CAMERA_VIDEO_ROTATION_90
                           (2): 180              - KMB_CAMERA_VIDEO_ROTATION_180
                           (3): 270              - KMB_CAMERA_VIDEO_ROTATION_270
  geometric-mode      : Operating mode of geometric correction
                        flags: readable, writable
                        Enum "KmbCamGeometrichMode" Default: 0, "off"
                           (0): off              - KMB_CAMERA_GEOMETRIC_MODE_OFF
                           (1): on               - KMB_CAMERA_GEOMETRIC_MODE_ON
  geometric-strength  : Control the amount of shading correction applied to the images
                        flags: readable, writable
                        Integer. Range: 1 - 10 Default: 0 
  hot-pixel-mode      : Set operational mode for hot pixel correction
                        flags: readable, writable
                        Enum "KmbCamHotPixelMode" Default: 0, "off"
                           (0): off              - KMB_CAMERA_HOT_PIXEL_MODE_OFF
                           (1): on               - KMB_CAMERA_HOT_PIXEL_MODE_ON
  ir-mode             : Infrared mode
                        flags: readable, writable
                        Enum "KmbCamIRMode" Default: 0, "on"
                           (0): on               - KMB_CAMERA_IR_MODE_ON
                           (1): off              - KMB_CAMERA_IR_MODE_OFF
                           (2): auto             - KMB_CAMERA_IR_MODE_AUTO
  isp-param-delay     : Number of frames after which to apply isp params
                        flags: readable, writable
                        Unsigned Integer. Range: 0 - 4294967295 Default: 0 
  isp-params          : ISP live tuning binary file
                        flags: readable, writable
                        String. Default: null
  legacy-band-stop-filter: Switch the band-stop filter of a camera sensor on or off, or specify its strength. Such band-stop filters can be used, for example, to filter out the fluorescent light component.
                        flags: readable, writable
                        Enum "KmbCamBandStopFilter" Default: 0, "off"
                           (0): off              - KMB_CAMERA_BAND_STOP_FILTER_OFF
                           (1): on               - KMB_CAMERA_BAND_STOP_FILTER_ON
  legacy-blue-balance : Blue chroma balance
                        flags: readable, writable
                        Integer. Range: -2147483648 - 2147483647 Default: 0 
  legacy-contrast     : Picture contrast or luma gain
                        flags: readable, writable
                        Integer. Range: -2147483648 - 2147483647 Default: 0 
  legacy-gamma        : Gamma adjust
                        flags: readable, writable
                        Integer. Range: -2147483648 - 2147483647 Default: 0 
  legacy-hue          : Hue or color balance
                        flags: readable, writable
                        Integer. Range: -2147483648 - 2147483647 Default: 0 
  legacy-red-balance  : Red chroma balance
                        flags: readable, writable
                        Integer. Range: -2147483648 - 2147483647 Default: 0 
  legacy-saturation   : Picture color saturation or chroma gain
                        flags: readable, writable
                        Integer. Range: -2147483648 - 2147483647 Default: 0 
  legacy-sharpness    : Adjusts the sharpness filters in a camera. The minimum value disables the filters, higher values give a sharper picture
                        flags: readable, writable
                        Integer. Range: -2147483648 - 2147483647 Default: 0 
  lens-aperture       : Size of the lens aperture
                        flags: readable, writable
                        Float. Range:   -3.402823e+38 -    3.402823e+38 Default:               0 
  lens-filter-density : State of lens neutral density filter(s)
                        flags: readable, writable
                        Float. Range:   -3.402823e+38 -    3.402823e+38 Default:               0 
  lens-focal-length   : Lens optical zoom setting
                        flags: readable, writable
                        Float. Range:               1 -    3.402823e+38 Default:               0 
  lens-focus-distance : Distance to plane of sharpest focus, measured from frontmost surface of the lens
                        flags: readable, writable
                        Float. Range:               0 -    3.402823e+38 Default:               0 
  lens-iris-position  : Iris position. 0 opened, 4 closed and 5 auto mode
                        flags: readable, writable
                        Integer. Range: 0 - 5 Default: 0 
  lens-optical-stabilization-mode: Whether optical image stabilization is enabled
                        flags: readable, writable
                        Enum "KmbCamOpticalStabilizationMode" Default: 0, "off"
                           (0): off              - KMB_CAMERA_LENS_OPTICAL_STABILIZATION_MODE_OFF
                           (1): on               - KMB_CAMERA_LENS_OPTICAL_STABILIZATION_MODE_ON
  message-forward     : Forwards all children messages
                        flags: readable, writable
                        Boolean. Default: false
  metadata-enable     : Enable metadata callbacks
                        flags: readable, writable
                        Boolean. Default: false
  metadata-send-tags  : Trigger for metadata tagging
                        flags: readable, writable
                        Boolean. Default: false
  multi-camera-ids    : Selected cameras' ids list: (comma separated values) where the first one is the main camera.
                        flags: readable, writable
                        String. Default: "0"
  multi-camera-mode   : Multi camera mode options: stereo, 360. To be used together with multi-camera-ids to select which cameras to be used.Default is stereo.
                        flags: readable, writable
                        String. Default: "none"
  multi-camera-sync   : Multi camera sync types: hw, sw. To be used together with multi-camera-mode to select which type of sensor sync should be used. Default is hw.
                        flags: readable, writable
                        Enum "KmbCamMulticamSync" Default: 0, "hw"
                           (0): hw               - KMBCAM_MULTICAMERA_SYNC_HW
                           (1): sw               - KMBCAM_MULTICAMERA_SYNC_SW
  name                : The name of the object
                        flags: readable, writable
                        String. Default: "kmbcamsrc0"
  noise-reduction-mode: Mode of operation for the noise reduction algorithm
                        flags: readable, writable
                        Enum "KmbCamNoiseReductionMode" Default: 0, "off"
                           (0): off              - KMB_CAMERA_NOISE_REDUCTION_MODE_OFF
                           (1): on               - KMB_CAMERA_NOISE_REDUCTION_MODE_ON
  noise-reduction-strength: Control the amount of noise reduction applied to the images
                        flags: readable, writable
                        Integer. Range: 1 - 10 Default: 0 
  num-frames          : Number of frames to output before sending EOS (-1 = unlimited)
                        flags: readable, writable
                        Integer. Range: -1 - 2147483647 Default: -1 
  parent              : The parent of the object
                        flags: readable, writable
                        Object of type "GstObject"
  raw-enable          : Enable raw input usage
                        flags: readable, writable
                        Boolean. Default: false
  raw-format          : Property to choose a format for raw input. Supported formats are:
        BGGR10, GBRG10, GRBG10, RGGB10,
        BGGR10P, GBRG10P, GRBG10P, RGGB10P,
        BGGR12, GBRG12, GRBG12, RGGB12,
        BGGR12P, GBRG12P, GRBG12P, RGGB12P.
The default is RGGB12.
                        flags: readable, writable
                        String. Default: "BGGR10"
  raw-height          : Raw input image height
                        flags: readable, writable
                        Unsigned Integer. Range: 0 - 4294967295 Default: 1964 
  raw-location        : Dir containing raw input images. Ex. /raw_img
                        flags: readable, writable
                        String. Default: "/raw_input_images"
  raw-name-prefix     : Prefix of raw input images' names. Ex. img
                        flags: readable, writable
                        String. Default: "img"
  raw-width           : Raw input image width
                        flags: readable, writable
                        Unsigned Integer. Range: 0 - 4294967295 Default: 2616 
  scanline-align      : Scanline alignment
                        flags: readable, writable
                        Unsigned Integer. Range: 1 - 4096 Default: 1 
  scene-mode          : Scene mode works as a preset for different image capture mode settings
                        flags: readable, writable
                        Enum "KmbCamSceneMode" Default: 0, "auto"
                           (0): auto             - KMB_CAMERA_SCENE_MODE_AUTO
                           (1): action           - KMB_CAMERA_SCENE_MODE_ACTION
                           (2): portrait         - KMB_CAMERA_SCENE_MODE_PORTRAIT
                           (3): landscape        - KMB_CAMERA_SCENE_MODE_LANDSCAPE
                           (4): night            - KMB_CAMERA_SCENE_MODE_NIGHT
                           (5): night-portrait   - KMB_CAMERA_SCENE_MODE_NIGHT_PORTRAIT
                           (6): theatre          - KMB_CAMERA_SCENE_MODE_THEATRE
                           (7): beach            - KMB_CAMERA_SCENE_MODE_BEACH
                           (8): snow             - KMB_CAMERA_SCENE_MODE_SNOW
                           (9): sunset           - KMB_CAMERA_SCENE_MODE_SUNSET
                           (10): steadyphoto      - KMB_CAMERA_SCENE_MODE_STEADYPHOTO
                           (11): fireworks        - KMB_CAMERA_SCENE_MODE_FIREWORKS
                           (12): sports           - KMB_CAMERA_SCENE_MODE_SPORTS
                           (13): party            - KMB_CAMERA_SCENE_MODE_PARTY
                           (14): candlelight      - KMB_CAMERA_SCENE_MODE_CANDLELIGHT
                           (15): barcode          - KMB_CAMERA_SCENE_MODE_BARCODE
  sensor-exposure-time: Control the amount of noise reduction applied to the images
                        flags: readable, writable
                        Integer64. Range: 0 - 30000000000 Default: 0 
  sensor-frame-duration: Duration from start of frame exposure to start of next frame exposure
                        flags: readable, writable
                        Integer64. Range: -9223372036854775808 - 9223372036854775807 Default: 0 
  sensor-sensitivity  : Gain applied to image data. Must be implemented through analog gain only if set to values below 'maximum analog sensitivity'. If the sensor can't apply this exact gain, it should lessen the gain to the nearest possible value (rather than gain more).
                        flags: readable, writable
                        Integer. Range: -2147483648 - 2147483647 Default: 0 
  shading-mode        : Quality of lens shading correction applied to the image data
                        flags: readable, writable
                        Enum "KmbCamShadingMode" Default: 0, "off"
                           (0): off              - KMB_CAMERA_SHADING_MODE_OFF
                           (1): on               - KMB_CAMERA_SHADING_MODE_ON
  shading-strength    : Control the amount of shading correction applied to the images
                        flags: readable, writable
                        Integer. Range: 1 - 10 Default: 0 
  stride-align        : Stride alignment
                        flags: readable, writable
                        Unsigned Integer. Range: 1 - 4096 Default: 1 
  test-pattern        : Selected smart camera test pattern
                        flags: readable, writable
                        Enum "KmbCamTestPattern" Default: 3, "color_bars"
                           (0): repeating        - KMBCAM_TEST_PATTERN_REPEATING
                           (1): seed             - KMBCAM_TEST_PATTERN_REPEATING_SEED
                           (2): seed_ts          - KMBCAM_TEST_PATTERN_REPEATING_SEED_TS
                           (3): color_bars       - KMBCAM_TEST_PATTERN_COLOR_BARS
  tonemap-mode        : Table mapping for red, green, blue input values to output values
                        flags: readable, writable
                        Enum "KmbCamTonemapMode" Default: 0, "off"
                           (0): off              - KMB_CAMERA_TONEMAP_MODE_OFF
                           (1): on               - KMB_CAMERA_TONEMAP_MODE_ON
  transform-hub       : Transform hub property.
                        Supported values are: none, basic, full, stitching, EPTZ.
                        Transform hub full has 3 outputs: one with sensor resolution and two scaled.
                        Transform hub basic has 2 outputs: one with sensor resolution and one scaled.
                        The scaled outputs can be upscaled or downscaled.
                        flags: readable, writable
                        String. Default: "none"
  v4l2-debug-level    : Selected v4l2 debug level
                        flags: readable, writable
                        Unsigned Integer. Range: 0 - 4294967295 Default: 0 
  video-stabilization-mode: Whether video stabilization is active 
                        flags: readable, writable
                        Enum "KmbCamVideoStabilizationMode" Default: 0, "off"
                           (0): off              - KMB_CAMERA_VIDEO_STABILIZATION_MODE_OFF
                           (1): on               - KMB_CAMERA_VIDEO_STABILIZATION_MODE_ON

Children:
  auxiliary_3_source_raw
  auxiliary_3_source_5
  auxiliary_3_source_4
  auxiliary_3_source_3
  auxiliary_3_source_2
  auxiliary_3_source_1
  auxiliary_3_source_0
  auxiliary_2_source_raw
  auxiliary_2_source_5
  auxiliary_2_source_4
  auxiliary_2_source_3
  auxiliary_2_source_2
  auxiliary_2_source_1
  auxiliary_2_source_0
  auxiliary_1_source_raw
  auxiliary_1_source_5
  auxiliary_1_source_4
  auxiliary_1_source_3
  auxiliary_1_source_2
  auxiliary_1_source_1
  auxiliary_1_source_0
  source_raw
  source_5
  source_4
  source_3
  source_2
  source_1
  source_0
(END)

(END)

(END)